BRU2456000_01

Audio Widget

The Audio Widget is used to control audio related parameters such as volume, treble, bass, balance, and source for a given zone, using the C-Bus Audio Application. 

This Application works natively with the C-Bus Multi-Room Audio system, and is also supported by the C-Bus Automation Controllers where it can be used to integrate with third party Multi-Room Audio systems, to provide simple on-wall control from the C-Bus key unit, avoiding the need for an additional control.

Key Function

Description

Volume Up

Works like Dimmer Up, but for Volume.  Use for 2-key control of Volume.

Volume Down

Works like Dimmer Up, but for Volume. Use for 2-key control of Volume.

Volume Cycle

Works like Toggle Dimmer, but for Volume. Use for single key control of Volume.

Treble Up

Long press increases Treble. Short Press sets Treble to neutral. Use for 2-key control of Treble.

Treble Down

Long press decreases Treble. Short Press sets Treble to neutral. Use for 2-key control of Treble.

Treble Cycle

Long Press works like Toggle Dimmer, but for Treble. Short press returns Treble to neutral. Use for single key control of Treble.

Bass Up

Long press increases Bass. Short Press sets Bass to neutral. Use for 2-key control of Bass.

Bass Down

Long press decreases Bass. Short Press sets Bass to neutral. Use for 2-key control of Bass.

Bass Cycle

Long Press works like Toggle Dimmer, but for Bass. Short press returns Bass to neutral. Use for single key control of Bass.

Balance Left

Long press shifts Balance to left. Short Press sets Balance to centre. Use for 2-key control of Balance.

Balance Right

Long press shifts Balance to right. Short Press sets Balance to centre. Use for 2-key control of Balance.

Balance Cycle

Long Press works like Toggle Dimmer, but for Balance. Short press returns Balance to centre. Use for single key control of Balance.

Next Source

Short press selects next source

Previous Source

Short press selects previous source

Preset Source

Short press selects specified source

Dynamic 1

Short press sends Dynamic 1 message. The function of this depends on the Dynamic 1 function configured in the Matrix Switcher for the currently selected source.

Dynamic 2

Short press sends Dynamic 2 message. The function of this depends on the Dynamic 2 function configured in the Matrix Switcher for the currently selected source.

Status Indication

The indicator state for the Audio Widget is dependent on the variable it is controlling.

For Volume:

  • If the Volume is zero, the indicator will show the Off color defined for the Widget

  • If the Volume is not zero, the indicator will show the On color defined for the Widget

For Treble, Bass, and Balance:

  • If the value is at neutral/centre, the indicator will show the Off color defined for the Widget

  • If the value is not at neutral/centre, the indicator will show the On color defined for the Widget

For Preset Source:

  • If the current source is not equal to the source set by the preset, the indicator will show the Off color defined for the Widget.

  • If the current source is equal to the source set by the preset, the indicator will show the On color defined for the Widget.

For all other Key Functions the indicator will always show the On color defined for the Widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.