BRU2456000_01

Getting Started

The Next Generation Saturn and Saturn Zen wall plates need to be configured using the SpaceLogic C-Bus Commission Software before they can be used. 

To configure the units using SpaceLogic C-Bus Commission Software, you will need

  • A computer equipped with Windows 10 Professional (64-bit) or newer.

  • SpaceLogic C-Bus Commission Software.

  • Functional C-Bus network, consisting of at least:

    • A C-Bus Power Supply

    • A C-Bus interface such as a C-Bus PC-Interface, C-Bus Network Interface, or a C-Bus Automation Controller

    • Key unit to be configured

You may also need a USB Type-C cable if you wish to update the firmware in the key unit.

To download the software click here

Version

This user guide describes functionality of the unit according to the firmware version 1.1.0.

Installation Location

  • For indoor use only

  • Allow adequate ventilation

  • Do not cover the unit

  • Locate the wall plates as close as possible to C-Bus Power supplies to minimize any voltage drop

  • Avoid paint, stickers, or other decorations

  • If using the temperature sensor feature, consider the further recommendations mentioned in “Temperature and Humidity Sensors

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.