BRU2456000_01

Firmware Update

The SpaceLogic C-Bus Commission software will notify if a firmware update is required.

The update requires a connection to the USB-C connector on the rear of the unit, and is performed using the SpaceLogic C-Bus Commission software.

All required firmware files will be included and authenticated as part of the latest SpaceLogic C-Bus Commission software release.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.