BRU2456000_01

Shutter Relay Widget

The Shutter Relay Widget is specifically for use with the C-Bus Shutter Relay.

The Shutter Relay widget offers Key Functions for 1-key (Open-Stop-Close-Stop), 2-key (Open-Stop/Close-Stop), or 3-key (Open/Stop/Close) operation for C-Bus Shutter Relays configured for level translation mode.

Key Function

Description

Shutter Toggle

1 key shutter relay control for use with shutter relay level translation mode. Sends recall 98%.

Shutter Open/Stop

Open/Stop for 2 key shutter relay control for use with shutter relay level translation mode. Sends Recall 99%.

Shutter Close/Stop

Close/Stop for 2 key shutter relay control for use with shutter relay level translation mode. Sends Recall 1%.

Shutter Open

Open for 3 key shutter relay control for use with shutter relay level translation mode. Sends On.

Shutter Close

Close for 3 key shutter relay control for use with shutter relay level translation mode. Sends Off.

Shutter Stop

Stop for 3 key shutter relay control for use with shutter relay level translation mode. Sends Recall 2%.

Status Indication

The indicator state for the Shutter Relay Widget is based on the level of the group controlling the shutter relay, which is related to the position of the shutter/blind.

  • If the shutter/blind is closed, the level is zero, and the indicator will show the Off color defined for the Widget

  • If the shutter/blind is not closed, the level is not zero, and the indicator will show the On color defined for the Widget

It should be noted that for the Shutter Relay Widget, the indicator state relies on the Status Report to synchronize, which means it can take several seconds for the state to assume the correct value after the key is operated. This also means that for correct operation of the indicator for Shutter Relay Widgets, the Key Unit and the Shutter Relay must be on the same C-Bus network (indicators will not work correctly if there are any C-Bus Network Bridges between the Key Unit and the Shutter Relay).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.