BRU2456000_01

Sequence Widget

The Sequence Widget is used for interacting with a Sequence. 

Key Function

Description

Sequence Toggle

If sequence not already active, short press triggers sequence. If sequence is already active, short press turns off all lighting groups in sequence that are on.

Sequence Start

Triggers sequence.

Sequence Off

If sequence is already active, short press turns off all lighting groups in sequence that are on.

Sequence Reverse Toggle

If sequence not already active, short press triggers sequence. If sequence is already active, short press turns off all lighting groups in sequence that are on, in reverse order.

Sequence Reverse Off

If sequence is already active, short press turns off all lighting groups in sequence that are on, in reverse order.

Sequence Stop

If sequence is currently executing, stops execution.

Status Indication

The indicator state for the Sequence Widget indicates when the sequence is active:

  • If the sequence is active, the indicator will show the Off color defined for the Widget.

  • If the sequence is not active, the indicator will show the On color defined for the Widget.

Refer Sequence for more details on how the sequence's active status is determined.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.