BRU2456000_01

Linked Widget

The Linked Widget allows control of a group based on an event on another Widget (the “Control” widget).

The Linked Widget uses a “Linked Event” on the Control Widget to trigger a “Linked Action” on its own group.

Linked Event

Description

Control Widget turns on

Target level of the Control Widget changes from zero to non-zero as a result of a key event

Control Widget turns off

Target level of the Control Widget changes from non-zero to zero as a result of a key event

Timer Expires on Control Widget

A timer started by a key event on the Control Widget expires

Linked Action

Description

Turn On

If the Linked Widget group is Off, Turn on at the given level with the given ramp rate. No action if the Linked Widget group is already On.

Turn Off

If the Linked Widget group is On, Turn Off with the given ramp rate. No action if the Linked Widget group is already Off.

Preset

Sets the given level at the given ramp rate, regardless of the state of the Linked Widget group.

Turn On and Start Timer

If the Linked Widget group is Off, Turn on at the given level with the given ramp rate, and start a timer with the given timer parameters. If the Linked Widget group is already On, only the timer is started.

Turn Off and Start Timer

If the Linked Widget group is On, Turn off with the given ramp rate, and start a timer with the given timer parameters. If the Linked Widget group is already Off, only the timer is started.

Start Timer

Start a timer with the given timer parameters.

Trigger Event

Send a Trigger Event. If the Trigger Group and Action Selector match a local scene or sequence, these are triggered.

Enable Event

Sets an Enable Group to the Level provided.

The Control Widget must be a Linked Widget Actions which can also be enabled or disabled per profile.

Example Use Case: Fan Run-On Timer

On a 1-key Key Unit in a Toilet, the key is set up with a Lighting Widget with “Toggle” Key Function to control the light. A Linked Widget can be set up to also turn on the fan when then light is turned on, and a second Linked Widget can be set up to start a timer to turn the fan off after 5 minutes, when the light is turned off.

Widget

Type

Key Function

Group

1

Lighting

Toggle

Toilet Light

Widget

Type

Group

Control Widget

Linked Event

Linked Action

Result

2

Linked

Toilet Fan

1

Control Widget Turns On

Turn On

When the Toilet Light is turned on, this Linked Widget turns on Toilet Fan

3

Linked

Toilet Fan

1

Control Widget Turns Off

Start Timer (Timer Value =10 mins, Expiry Level = 0)

When the Toilet Light is turned off, this Linked Widget starts a timer to turn off the Toilet Fan in 10 minutes

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.