BRU2456000_01

Enable Widget

The Enable Widget is used for controlling groups on the Enable Control Application. This application is typically used to enable or disable functionality in other units, for example enabling or disabling a sensor, or selecting a Profile.

As such there are a much more limited number of Key Functions used with the Enable Widget.

Key Function

Description

Toggle

Short press toggles state between on and off with instant ramp.

On

Turns group on with instant ramp, only if currently off.

Off

Turns group off with instant ramp, only if currently on.

Preset

Short press recalls preset level with instant ramp, regardless of current level. Long Press ramps to off if on.

Preset on Short Press

Short Press recalls the preset level with instant ramp.

Preset on Long Press

Long Press recalls the preset level with instant ramp.

Unused

Key does nothing. Useful to indicate status only.

Status Indication

The status of the indicator is based on the level of the group address controlled:

  • If the level of the group address is not equal to the Preset level, the indicator will show the Off color defined for the Widget

  • If the level of the group address is equal to the Preset level, the indicator will show the On color defined for the Widget

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.