BRU2456000_01

Multi-Toggle Widget

The Multi-Toggle Widget is designed specifically to perform a Toggle function on multiple groups.

The state of the Multi-Toggle Widget is,

  • off: if all of the groups controlled by the Widget are off

  • on: if any of the groups controlled by the Widget are on (level)

Having said that, the Toggle function works to Toggle the state of all the groups controlled by the widget to the new state. So if any group controlled by the Widget is on, pressing the Key will send an ‘Off’ command to all of the groups. Conversely, if all of the groups controlled by the Widget are off, pressing the key will send an ‘On’ command to all of the groups in the Widget.

A common use case for this would be a master bedroom, where there is a switch at each side of the bed, which controls that side's bedside lamp, as well as the main room lights. There is also a switch by the door, where a key can be assigned to a Multi-Toggle Widget configured to control all of the lights in the room. If, when leaving the room, any of the lights in the room are on, the Multi Toggle key will turn them off.

Status Indication

The indicator state for the Multi-Toggle Widget is based on the state of the widget as defined above.

  • If the state is Off, the indicator will show the Off color defined for the Widget.

  • If the state is On, the indicator will show the On color defined for the Widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.