BRU2456000_01

Configure the Device

Configuration and Commissioning of the C-Bus unit is done by the C-Bus connection using the “SpaceLogic C-Bus Commission” software. To download the software click here

The unit can be powered up by the USB-C connection for programming via C-Bus (without an energized mains connection).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.