BRU2456000_01

Safety Precautions

WARNING
INCORRECT C-BUS CABLE INSTALLATION
The C-Bus network cabling is classified as Separated Extra-Low Voltage (SELV) wiring. To maintain this requirement, the approved C-Bus cable must be used.
  • Ensure that adequate separation and/or segregation of the C-Bus cable from other wiring (for example Low Voltage wiring) is maintained throughout the entire installation.
  • Ensure the C-Bus network cable is installed in accordance with the SELV wiring rules and regulations of the jurisdiction.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
Incorrect C-Bus installation location
To prevent the possibility of intentional or unintentional interference with the configuration or operation of the C-Bus installation, this equipment should be installed in a location with appropriate access control.
Failure to follow these instructions can result in equipment damage.

Megger Testing

NOTICE
megger testing
Megger testing must never be performed on any cable while connected to the product as it could degrade the performance of the product and/or the network.
Failure to follow these instructions can result in equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.