BRU2456000_01

Scene Widget

The Scene Widget offers the traditional scene Key Function of Scene Set, as well new

  • “Scene Modify” Key Functions Scene Off (which turns off all groups that were turned on in an active scene)

  • Scene Toggle (where a single key alternately performs Scene Set and Scene Off)

  • Scene On/Up and Scene Off/Down (where a short presses perform the Scene Set/Scene Off and long presses ramp the groups that are on in the scene)

These new “Scene Modify” Key Functions only work on scenes contained within the unit.

Key Function

Description

Scene Toggle

If scene not already active, short press triggers scene. If scene is already active, short press turns off all groups in scene that are on.

Scene Set

Short press triggers scene.

Scene Off

If scene is active, short press turns off all groups in scene that are on. No effect if scene is inactive.

Scene Off/Down

If scene is active, short press turns off all groups in scene that are on. If scene is active, long press ramps all group in scene down at specified ramp rate. No effect if scene is inactive.

Scene On/Up

Short press triggers scene. If scene is active, long press ramps all group in scene up at specified ramp rate.

Status Indication

The indicator state for the Scene Widget indicates when the scene is active:

  • If the scene is active, the indicator will show the Off color defined for the Widget.

  • If the scene is not active, the indicator will show the On color defined for the Widget.

Refer Scenes for more details on how the scene's active status is determined.

Scene Repair

The "Scene Repair" feature can also be enabled. When enabled, Scene Repair will reinstate the “Active” status of the scene if all groups in the scene are returned to the levels as defined by the scene.

This can be useful to achieve correct scene indication where room level scenes are used but are set as part of a larger overall scene.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.