BRU2456000_01

Fan Control Widget

The Fan Control Widget is specifically for use with the C-Bus Sweep Fan Control Relay. 

There are no Key Functions to set for the Fan Control Widget. Each Short Press sends a Trigger Control message to trigger the Sweep Fan Control Relay to cycle to the next speed.

The Trigger Group, Action Selector, and Group Address configured should match the settings in the C-Bus Sweep Fan Control relay(s) to be controlled. The Group Address specified is used to indicate the status of the fan.

Status Indication

The indicator state for the Fan Control Widget is based on the level of the group controlling the fan.

  • If the fan is Off, the indicator will show the Off color defined for the Widget.

  • If the fan is On, the indicator will show the On color defined for the Widget.

IMPORTANT: For correct operation of the indicator for Fan Control Widgets, the Key Unit and the Sweep Fan Control Relay must be on the same C-Bus network (indicators will not work correctly if there are any C-Bus Network Bridges between the Key Unit and the Sweep Fan Control Relay).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.