DOCA0256FR-01

About the Document

Document Scope

This guide provides users, installers, and maintenance personnel with the technical information needed to operate the PROFIBUS DP protocol on the LTMT main unit.

This guide is intended for:

  • Design engineers

  • System integrators

  • Maintenance engineers

Validity Note

This guide is valid for the following LTMT main units:

  • LTMTPFM: LTMT main unit with PROFIBUS DP protocol, 100–240 Vac/Vdc

  • LTMTPBD: LTMT main unit with PROFIBUS DP protocol, 24 Vdc

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Product Related Cybersecurity Information

Environmental Data

For product compliance and environmental information, refer to the Schneider Electric Environmental Data Program.

Available Languages of the Document

The document is available in these languages:

  • English

  • Chinese

  • French

  • German

  • Italian

  • Korean

  • Spanish

Related Documents

Title of documentation

Description

Reference number

TeSys Tera Motor Management System User Guide

This is the main user guide that introduces the complete TeSys Tera system. It describes the main functions of the LTMT main units, LTMTCT/LTMTCTV sensor modules, LTMT expansion modules, and LTMTCUF control operator unit.

DOCA0257EN

TeSys Tera Motor Management System Installation Guide

This guide describes the installation, commissioning, and maintenance of the LTMT main unit, LTMTCT/LTMTCTV sensor modules, LTMT expansion modules, and LTMTCUF control operator unit.

DOCA0356EN

TeSys Tera Motor Management System LTMTCUF control operator unit User Guide

This guide describes how to install, configure, and use the LTMTCUF control operator unit.

DOCA0233EN

TeSys Tera Motor Management System DTM library Online Help Guide

This guide describes the TeSys Tera DTM Library which allows the customization of the control functions of the TeSys Tera Motor Management System.

DOCA0275EN

TeSys Tera Motor Management System DTM library Software Release Notes

This document provides important information about the TeSys Tera DTM Library software and provides summary of new features and enhancement.

DOCA0279EN

TeSys Tera Motor Management System Firmware Release Notes

This guide provides important information about the TeSys Tera system firmware packages and provides summary of new features and enhancement.

DOCA0276EN

Electrical Installation Guide (wiki version)

The aim of the Electrical Installation Guide (and now wiki) is to help electrical designers and contractors to design electrical installations according to the standards such as the IEC 60364 or other relevant standards.

www.electrical-installation.org

TeSys Tera Motor Management System EtherNet/IPGuide

This guide describes the EtherNet/IP network protocol communication of the LTMT main unit.

DOCA0258EN

TeSys Tera Motor Management System Cybersecurity Guide

This guide provides information on cybersecurity aspects for the TeSys Tera Motor Management System. This guide addresses on how to secure your operational technology network, or your company serial or Ethernet network.

DOCA0260EN

To find documents online, visit the Schneider Electric download center (www.se.com/ww/en/download/).

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Trademarks

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.