System User Guide Wiser Home (Germany, Austria) - 11

Reduce my Bill - Basic Optimisation

IMPORTANT: Reduce my bill feature is available only in Australia, France, German, Spain and Portugal.

This feature automatically schedule your loads when the cost is the cheapest. Shifting loads at low tariff periods reduces the energy bill. Based on your tariff input, enabling this feature will automatically switch your high-consuming devices ON during the cheapest electricity rates and OFF during peak hours.

IMPORTANT: While the feature is active, Reduce My Bill schedules replace any customized schedules.

Supported devices:

  • Power Micromodule (Water Heater)

  • EVLink Home Smart

  • Schneider Charge

Pre-requisite

Once device is commissioned and the tariff is set, user gets notified in the Insights tab that this feature is available and also a push-notification is sent.

Enabling Basic Optimisation

To enable Basic Optimization:

  1. On the Home screen, tap Energy > Insights then tap banner (A).

    IMPORTANT:
    • Do not accidentally close the banner as it takes 2 weeks for this option to reappear.

    • If you close the banner again, a final reminder will appear after 6 weeks.

  2. Read the tutorial information and tap Next twice, then tap Go to Reduce my Bill settings.

  3. Enable the toggle switch (A) for the devices you want to have this feature.

    IMPORTANT:
    • If you have closed the reminder banner, you can also enable the Basic Optimisation feature in the Settings screen.

      • On the Home screen, tap > Energy Management > Reduce My Bill and follow step 3.

    NOTE: After enrolling devices to Basic Optimisation, refer to Using Reduce My Bill to view how the devices are controlled and scheduled for usage.
    TIP: If you want to save further more, tap the banner (B) to explore Wiser Home AI and unlock advanced features. Refer to Wiser Home AI for detailed information.

Disabling Device from Basic Optimisation

To disable device from Basic Optimisation:

  1. On the Home screen, tap > Energy Management > Reduce my Bill.

  2. Disable the toggle switch for the devices you don’t want to have this feature.

    A notification window is prompted. Read the information.

  3. If you wish to proceed, tap Continue else tap Cancel.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?