SUG_DA_WH-04

Appliances

Wiser Power Micromodule

CCTFR6730

The Wiser Power Micromodule is for switching loads (up to 3000 W resistive) such as a hot water tank or a socket outlet.

In combination with the Wiser app, the energy consumption can be measured and the module can be used for load shedding or demand response.

LK product catalog

Instruction Sheet (PDF)

Device User Guide

LK FUGA® Wiser Wireless Battery 4 Button Switch

550D6001

550D0001

Control Wiser devices and Moments/Automations with a convenient remote controller.

A wireless battery switch can also be used as a remote controller in a Room Control system.

LK product catalog (with cover)

LK product catalog (without cover)

Instruction Sheet (PDF)

Device User Guide

LK FUGA® Wiser wireless Socket Outlet 1½ M

545D6115

545D0115

Remotely controls and monitors the power consumption of the plugged-in load.

LK product catalog (with cover)

LK product catalog (without cover)

Instruction Sheet (PDF)

Device User Guide

Wiser SmartPlug 16 A

CCT711119

Controls various electrical devices, for example floor lamps, radios, ventilators or coffee machines, using the app. Monitor energy consumption of plugged-in devices.

LK product catalog

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.