SUG_DA_WH-04

About Signal Strength

Zigbee® signal strength or RSSI (Received Signal Strength Indicator) indicates the signal quality between your devices and the Wiser hub. The Closer the RSSI value is to 0, the better the signal. For example, an RSSI of -50dBm is a good signal, while an RSSI of -80dBm indicates poor signal.

Signal Strength Indicator

There is four different levels of signal strength:

Good Signal (between 0 & -54dBm)

Normal Signal (between -54 & -79dBm)

Poor Signal (<-79dBm)

No Signal (device is offline)

Cause of Poor Signal

Connectivity issues can be caused by various factors, such as:

  • Distance between the hub and devices - the signal becomes weaker as the devices move farther apart.

  • Physical Obstructions - doors, walls, furniture, household appliances, especially with metal surfaces, and other electronic devices can weaken the Zigbee® signal.

Troubleshooting

  1. Place the hub into open space.

  2. Make sure you check if all powered devices are switched on and working normally.

  3. If possible, move the Wiser Hub closer to the device with signal issues.

  4. Try to remove any physical obstructions between the Wiser Hub and the device with poor or no signal.

Signal Extender

If you are still experiencing connectivity issues, we recommend adding lighting control devices such as a dimmer, switch, socket or blind control device etc. to your system. It has a built-in signal range extender that boosts the signal between your devices and the hub.

Help & Support

If you require further assistance, visit our Support Pages.

Help & Support:

For Denmark, Visit: https://www.se.com/dk/da/work/support/

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.