SUG_DA_WH-04

Adding a Device

You can add a new Device at any time.
NOTE:
  • The hub must be installed before adding a Wiser device.

  • Add mains-powered devices before battery-powered devices. Refer to Selecting the mounting location.

  • The instructions provided for adding the device are generic. Some steps may vary based on the device types. You can find detailed information in the Device User Guide of the respective device. Refer to List of Wiser Devices for the links to Device user guide for each devices.

  1. Tap (A) in the List of Devices.
  2. Find your device by navigating the categories at the top of the screen (B).
  3. Tap the type of Device (C) you want to add and follow the instruction in the app.
  4. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    IMPORTANT:
    1. The QR code scanning is not applicable to following devices.

      Device

      • EV Link Home Smart

      • PowerTag Energy

      • Schneider Charge

      • Wiser Plug

      • Wiser Radiator Thermostat

      • Wiser Room Thermostat

      • Wiser Underfloor Heating Controller / Connection Strip

    2. If you are facing difficulties in scanning the QR code, refer to Handling QR code Issues.
  5. Tap Next.
  6. Set the Device into pairing mode.

    The Wiser Home App will guide you through the pairing process. You can find detailed information about the pairing mode in the Device User Guide of the respective device. Refer to List of Wiser Devices for the links to Device user guide for each devices.

    When the pairing is complete, you can give the device a name.

  7. Enter a name for the Device.
  8. Tap Next.
  9. Assign the Device to an existing Room or create a new Room by entering a name in the field.
  10. Tap Submit.
  11. Configure the dimmer settings, such as dimming mode, power-on behavior, and brightness level, according to your preferences, then tap Submit.

You can now control the Device with the Wiser Home App. You can find detailed information about controlling your Devices in chapter Controlling the Wiser System

NOTE: Depending on the type of Device, there are further features available. You can find detailed information in the Device User Guide of the respective device. Refer to List of Wiser Devices for the links to Device user guide for each devices.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.