SUG_DA_WH-04

Editing an Automation

On the Automation screen (A):

  1. Tap the Automation you want to edit (B).

On the Edit Automation screen, you can:

  • Change the icon.

  • Rename the automation.

  • Change the condition, time or action.

To change the condition, time or action of an Automation:

  1. Navigate to the relevant tab (If/When/Then) and tap the condition, time or action you want to change.

  2. Set the new values.

  3. Tap Save (C).

To remove a condition, time or action:

  1. Navigate to the relevant tab.

  2. Swipe the relevant condition, time or action left.

  3. Tap the (A)

  4. Tap Save (B).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?