SUG_DA_WH-04

Moments

Create a Moment to change the state of multiple devices with a single tap. Moments act like scenes, allowing you to control several devices all at the same time.

Moments are created and edited on the Automation screen (A)

A

Navigate to the automations screen.

B

Activate a Moment.

C

Rearrange the order of Moments.

Also affects the list on the Home Screen.

D

Edit a Moment.

E

Add a Moment

NOTE:
  • A Moment will only set the status of devices. In order to put the affected devices in another status, you need to change it manually or create a reversing Moment.

  • If you added a Climate device to the Moment, you can reverse the change of the Climate device by tapping Cancel all overrides.

  • If a device follows a Schedule, the Moment of that device will only last to the next scheduled setting.

Moments can also be assigned to push buttons of specific devices (e.g. Connected Wireless Switch). Find more information about this feature in the respective device user guide. Refer to List of Wiser Devices for the links to Device user guide for each devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.