SUG_DA_WH-04

Compatible Wiser Devices for Matter Bridge

Following are the Matter bridge compatible devices:

Refer to List of Wiser Devices for the links to Device user guide for each devices.

Sensors

Wiser Window/Door Sensor

Wiser Water Leakage Sensor

Wiser Motion Sensor

Wiser Temperature/Humidity Sensor

Lights

Wiser Micro Module Light Switch

Connected Relay Switch 10 A

LK® Wiser Push-Button Switch
LK® FUGA Wiser Push-Button Switch

Dimmers

Wiser Micro Module Dimmer
Wiser Multiwire Micro Module LED Dimmer


LK® FUGA Wiser Multiwire LED Push-button Dimmer
LK® Wiser Multiwire LED Rotary Dimmer
LK® FUGA Wiser Multiwire LED Rotary Dimmer

Shutters

Wiser Micro Module Shades Control

Appliances

SmartPlug 16A

LK FUGA® Wiser wireless Socket Outlet 1½ M
LK FUGA® Wiser Wireless Battery 4 Button Switch

Climate

Wiser Radiator Thermostat

Wiser Room Thermostat

Wiser Underfloor Heating Connection Strip

Wiser 16 A Relay for Temperature Control

Safety

Wiser Smoke Alarm - Battery

Wiser Smoke Alarm 230 V

Energy

PowerTag E

PowerTag C

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.