SUG_DA_WH-04

Managing Favourites

Quickly access and control your most frequently used devices from the Home screen. You can also rearrange the devices as per your preference.

Add Favourites

  1. On the Home screen, tap Add favourites.

  2. Tap the icon to add all your favourite devices.

  3. Once complete, tap Done.

Now you can view all your favourite devices in the Home Screen.

Edit Favourites

  1. On the Home screen > Favourite devices, tap Edit.

  2. You can perform following actions:

    • Drag and drop to reorder your favourite devices.

    • Tap Manage favourites to add or remove the device from the favourites list.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.