SUG_DA_WH-04

List of Devices

In the Devices page, you can find all installed Devices of your Home, sorted by their device type.

The Devices will also display their Name, their Room location and, if applies, other information, e.g. the charge level of the battery and the indication of zigbee signal strength.

Tap a Device in the List to navigate to the Device Details.

  1. Login to the app.
  2. On the Home Screen, tap .
  3. Tap Devices.
List of Devices:

A

The battery charge level indicator which displays the current battery status for battery-powered devices.

B

Tap/click on the banner to get details about devices experiencing signal issues. Refer to Device With Signal Issues for details on devices facing the signal issues and refer to About Signal Strength to know more about the Zigbee® signal strength.

C

Hub Wi-Fi® signal strength indicator which displays your hub’s connection to your Wi-Fi® network. When the indicator displays , it signifies that there is no signal or connection.

D

Zigbee® signal strength indicator which displays the current signal strength of the zigbee devices.

NOTE: This feature is not applicable for Wiser Plug device.

E

Tap/click to add new devices.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?