SUG_DA_WH-04

Safety & Security

Wiser Smoke Alarm - Battery

CCT599002

The Wiser Smoke Alarm - Battery uses a photoelectric sensor to detect smoke generated by fire. It also includes a temperature sensor that detects heat caused by rapid increase in temperature. When connected to the Wiser system, the device sends notifications to the user via the Wiser app.

LK product catalog

Instruction Sheet (PDF)

Device User Guide

Wiser Smoke Alarm 230 V

CCT599502

550B1028

The Wiser Smoke Alarm 240 V Square uses a photoelectric sensor to detect smoke generated by fire and a temperature sensor that detects heat caused by rapid increase in temperature. It also includes a backup battery that allows the device to work if the power supply is disconnected. When connected to the Wiser system, the device will send notifications via the Wiser app.

LK product catalog , CCT599502
LK product catalog , 550B1028

Instruction Sheet (PDF) , CCT599502
Instruction Sheet (PDF) , 550B1028

Device User Guide

Wiser Window/Door Sensor

CCT591012

550B1023

Can be used to detect if a door or window is opened or closed.

LK product catalog , CCT591012
LK product catalog , 550B1023

Instruction Sheet (PDF),CCT591012
Instruction Sheet (PDF), 550B1023

Device User Guide

Wiser Motion Sensor

CCT595012

550B1022

Reports the detection of movement and measures the luminance of the environment.

Wiser Water Leakage Sensor

CCT592012

550B1021

Detects water on a surface.

LK product catalog , CCT592012
LK product catalog , 550B1021

Instruction Sheet (PDF), CCT592012
Instruction Sheet (PDF), 550B1021

Device User Guide

Wiser Temperature/Humidity Sensor

CCT593012

550B1024

Measures temperature and humidity

LK product catalog , CCT593012
LK product catalog , 550B1024

Instruction Sheet (PDF), CCT593012
Instruction Sheet (PDF), 550B1024

Device User Guide

ARGUS Motion Sensor Outdoor 360

CCT564114

CCT564119

It offers advanced motion detection, LUX measurement, and temperature sensing capabilities. It allows you to automate and enhance your smart home environment effortlessly.

LK product catalog, CCT564114
LK product catalog, CCT564119

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.