SUG_DA_WH-04

Room Details

In the Room details screen, you can check and change Room specific options, like a list of Devices assigned to a Room or changing the name of the Room.

Some devices have specific options and settings. For example Open Window Detection, when a Radiator Thermostat is assigned to the Room. You can find detailed information in the Device User Guide of the respective device. Refer to List of Wiser Devices for the links to Device user guide for each devices.

Tap a Device to navigate to the Device Options.

In the List of Rooms:

  1. Tap a Room (A).

Room Details:

A

Tap to change the name of the room

B

Zigbee® Signal strength indicator which displays the current signal strength of the Zigbee® devices. Refer to About Signal Strength to know more about the Zigbee® signal strength.

NOTE: This feature is not available for the Wiser Plug device.

C

Tap to delete the room.

NOTE:
  • Deleting a Room should not be necessary after you set up your Home, but you can do so at any time.

  • When you delete a Room, all the devices (except the climate device) assigned to that room will be listed as Unassigned in the Home screen.

D

The battery charge level indicator which displays the current battery status for battery-powered devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.