DUG_Underfloor Heating Connection Strip_WH-07

For your safety

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Safe electrical installation must be carried out only by skilled professionals. Skilled professionals must prove profound knowledge in the following areas:
  • Connecting to installation networks.
  • Connecting several electrical devices.
  • Laying electric cables.
  • Safety standards, local wiring rules and regulations.
Failure to follow these instructions will result in death or serious injury.
WARNING
HAZARD OF ELECTRIC SHOCK
  • The UFH connection strip is only for fixed wiring.
  • After wiring please ensure that the cables are:
    – correctly connected
    – fully inserted
    – firmly in position
    – not twisted or under tension
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?