DUG_Infrascan Outdoor Motion Sensor 360_WH-00

About the device

The Infrascan Outdoor Motion Sensor 360 (hereinafter referred to as motion sensor) detects nearby movement and measures the luminance of the environment to control the on/off function of the connected load or paired micro module. When motion is detected and the environment is darker than the set light level, the load will be turned on for the specified duration, starting from the last detection.

It can also control micro modules through a Quick Home Connection. In this setup when the motion is detected, the loads and the micro modules connected to the motion sensor turn on/off together.

Functionalities and features:

  • Expandable Connectivity: 1 motion sensor can connect with 3 Micro modules via Quick Home Connection.

  • Efficient Multi-Device Connection: 5 motion sensors can be linked to 1 Micro module via Quick Home Connection, maximizing convenience and efficiency.

  • Customized Sensitivity: Tailor the sensitivity of the device to suit your needs for precise control.

  • Adaptable LUX settings: Adjust the threshold of the light level to validate the detection.

  • Flexible Time Settings: Easily adjust the duration for which the load stays on after motion is detected to accommodate your schedule and preferences.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?