DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Changing the location

Using the Wiser Home app, you can change the location of the motion sensor.

To change the location:
  1. On the Device Details screen, tap of Location.
  2. On setup page, you can enter New room name (A) or select an existing room from the list (B).
    TIP: If the device is already assigned, you can tap Remove from Room (C) to remove it from the existing room.
  3. Once changes are done, tap Submit (D) to confirm the location of the motion sensor.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?