DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Setting the motion detection timer

Using the Wiser Home app, you can set the time of operation of a device after motion detection.

To set the motion detection timer:
  1. On the Device Details screen, tap Motion Detection Timer.
  2. Select one of the following modes:
    • Test Mode: To test the motion sensor and make sure that its placement and detection range are as required.

      NOTE: In this mode, the device connected to the motion sensor turns ON for 2 seconds after motion detection and then goes OFF for 3 seconds. If the motion is still detected after these 5 seconds, the device turns ON again.
    • Short Pulse: For devices which needs a short activation to complete an action like triggering an alert or capturing a photo.

      NOTE: In this mode, the device connected to the motion sensor turns ON for 1.5 seconds after motion detection and then goes OFF for 8.5 seconds. If the motion is still detected after these 10 seconds, the device turns ON again.
    • Custom Duration: To manually set the duration for which the device should operate after a motion detection.

      NOTE: The default time of operation of the device connected to the motion sensor after motion detection is 60 seconds. You can select the required time by selecting this option.
  3. If you tap Custom Duration you can:
    • Select a time period from the list ranging from 15 sec to 5 min

      or
    • Tap on Specific time to choose a time apart from the list.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?