Device settings
| Time setting |
Time setting: Adjusts the duration for which the sensor activates or triggers the connected load after detecting motion. NOTE: You can
also change the status of the load before the set time expires. For
more details on controlling the load's behavior, refer to Override modes.
|
|
| Short Pulse NOTE: Short Pulse can only be triggered every 10 s.
|
||
| 5s - 1hr (Logarithmic scale): Set the duration for which the connected load stays ON after motion is detected. When time expires, the connected load will turn off automatically. | ||
| Test: Test the sensitivity setting. The Load turns ON
for 2 s each time a motion is detected. The brightness setting will
be ignored. NOTE: Test can only be triggered every
5 s.
|
||
| LUX setting | LUX setting: Sets the ambient brightness threshold at which the sensor activates or triggers the connected load. When set to a specific lux level, the sensor will initiate its operation when the ambient brightness falls below the threshold level. | |
| 1-2000 Lux |
||
| Day mode |
||
| Teach in Threshold When this setting is selected, the current ambient brightness will be saved as the threshold after 15 seconds, giving time for the installer to step back and capture the correct brightness. The sensor will then use this saved brightness level as a reference for triggering the load. |
||
| Sensitivity |
Determines the detection range by adjusting the sensor's
sensitivity level. The higher the sensitivity, the more the detection
range. |
|
| Setup/Reset |
|