DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Setting the lux level

Using the Wiser Home app, you can set the motion sensor's lux level.

Lux level is the surrounding light intensity. Below the threshold lux level, when motion is detected, the devices associated with the motion sensor gets activated.


To adjust the lux level:

  1. On the Device Details screen, tap Lux level.
  2. Select one of the following modes:
    • Day Mode: For the devices which should be active during the days and the nights. The device operates irrespective of any lux value.

    • Night Mode: For the devices which should be active in low light conditions. The device operates when the lux level is below 300.

      NOTE: This mode is commonly used for outdoor lights.
    • Custom Lux Value: This allows the manual setting of the threshold lux level (from 0 to 2000).

  3. If you tap Custom Lux Value, drag the slider (A) right/left to adjust the threshold lux level.
  4. Tap Set.
    TIP: You can tap Use the current lux value to set the current ambient light intensity as the threshold lux level. The set threshold lux level will not be more than 2000.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.