DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Editing an automation

Using Wiser Home app, you can edit the existing automations.

To edit an automation:
  1. On the Home screen, tap .
  2. Go to Automation tab.
  3. Select the automation you want to edit.
  4. You can now perform following changes:
    • Change the icon.

    • Rename the automation.

    • Tap each condition to change the settings.

      • To remove a condition, slide the condition towards left and then tap (A) to delete it.

      • Tap Add conditions (B) to add new condition.

  5. Tap Save to save the changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?