DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Controlling the motion sensor

Using the Wiser Home app, you can:
  • See if the motion sensor is occupied or unoccupied.

  • Set the time for which a device connected to the motion sensor should operate after motion detection.

  • Manage the state (ON/OFF or open/close) of the device connected to the motion sensor.


To control the device connected to the motion sensor:
  1. On the Control tab, tap All devices or a room tab where the motion sensor is located.
    NOTE: If you only have a single device in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.
  2. Select the required motion sensor from the list (A).
  3. Select the time for which the connected device should operate.
  4. If required, tap on the device icon to activate or deactivate it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?