DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Pairing Micro Module with Motion Sensor

To pair a micro module to the motion sensor:
IMPORTANT: Micro module must be a Wiser Micro Module Dimmer, Wiser Micro Module Light Switch or Wiser Multiwire Micro Module LED Dimmer.
  1. Short press the mechanical push-button 5 times in quick succession.
    The status LED blinks green on the micro module LED.
    NOTE: If the micro module is located behind the mechanical push-button, the status LED is not visible.
  2. Open the cover of the motion sensor and short press the S/R (setup/reset) button 5 times in quick succession.
    • The status LED blinks green for few seconds.

    • When successfully paired, the status LED on the micro module and the motion sensor turns off.

    The load can now be controlled by the motion sensor.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?