Configuring the motion sensor
-
Tap Devices > Outdoor Motion Sensor and select the motion sensor which you want to configure.
TIP: You can also open device details screen by tapping on Device settings on the device control screen.
A |
Device Name: Tap to change the name of the device. |
B |
Location: Tap to assign a location for the motion sensor. Refer to Changing the location for more details on how to set the location. |
C |
Sensitivity: Tap to define the detection range of the motion sensor. Higher the sensitivity, more the detection range. Refer to Setting the sensitivity for more details on how to set sensitivity. |
D |
Motion Detection Timer: Tap to manage the operation time of a device after motion detection. Refer to Setting the motion detection timer for more details on how to set the lux level. |
E |
Lux Level: Tap to define threshold light intensity below which the connected load shall be activated. Refer to Setting the lux level for more details on how to set the lux level. |
F |
Motion Sensor LED: Tap the toggle switch (G) to allow the LED on the motion sensor to turn ON/OFF when motion is detected by the motion sensor. |
G |
Notify me if motion detected: Tap the toggle switch (H) to turn the notification ON/OFF. When it is ON and the motion is detected by the motion sensor, you get the notifications in the Wiser Home app. |
H |
Identify: Tap to find the location of the motion sensor in the room. NOTE: Upon identification of the motion
sensor, the status LED on it blinks.
Tap OK after identifying the motion sensor. |
I |
Delete: Tap to remove a motion sensor from the Wiser Home app. NOTE: After deleting, the motion sensor to
operate being independent of the settings made in the Wiser Home app.
|