DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Setting the sensitivity

Using the Wiser Home app, you can manage the sensitivity to define the detection range of the motion sensor.

To set the sensitivity:
  1. On the Device Details screen, tap Sensitivity.
  2. Drag the slider (A) left/right.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?