DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Checking the history

By using the Wiser Home app, you can check the history of motion detection events and temperature.

To check the history:
  1. On the Control tab, tap All devices or a room tab where the motion sensor is located.
  2. Select the required motion sensor from the list (A).
  3. Tap History (B).
  4. Tap any of the following options:
    • Temperature: To see the history of temperature.

    • Motion: To see the history of motion detection events.

    TIP: Tap Load More to see 100 more events.
    History of motion detection events of last 30 days and temperature of last one year can be checked.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?