DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Using the motion sensor

The following image shows the details available on the device control screen:

A

Current lux value.

B

Current temperature.

C

Current state of the device connected to the motion sensor and the instruction to operate it.
For example:

  • If the sensor controls the door/gate, you can set it to Open/Close.

  • If the sensor controls the devices like lights, you can set it to On/Off.

D

Current state of the motion sensor.
When the motion is detected by the motion sensor, it displays Occupied, otherwise it displays Unoccupied.

E

Option to monitor the history of motion detection and temperature.

F

Option to access the Device Details screen to update the motion sensor configuration.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?