DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Creating a moment

Moment allows you to group multiple actions that are usually performed together. By using the Wiser Home app, you can create moments.

To create a moment:
  1. On the Home screen, tap .
  2. Go to Moment > to create a moment.
  3. Enter the name of the moment (A).
  4. Tap Add actions (B) to select the list of devices.
  5. In the Select devices page, select the devices to be operated by the moment from the list (C).
  6. Tap Label.
  7. On the Moment creator page, tap Outdoor Motion Sensor to set it On/Off or Open/Close.
    For example:
    • If the sensor controls the door/gate, you can set it to Open/Close.

    • If the sensor controls the devices like lights, you can set it to On/Off.

  8. Tap Set.
  9. On the Moment creator page, tap Save.
    The moment will be visible on the Moments tab. You can tap on the moment to enable it.
    TIP:
    • If you want to see the created moments on the Home screen, go to Home > > Home screen > Moments. Enable the toggle button to view moments on the Home screen.

    • You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.

  10. To change the icon of the moment, tap the icon (D), select the required icon and tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?