DUG_Infrascan Outdoor Motion Sensor 360_WH-00

Editing a moment

Using Wiser Home app, you can edit the existing moment.

To edit a moment:
  1. On the Home screen, tap .
  2. Go to Moments, select the moment you want to edit and tap .
  3. On the Moment editor page, you can now perform following changes:
    • Change the icon.

    • Rename the moment.

    • Tap each action to change the settings.

      • To remove a action, slide the action towards left and then tap (A) to delete it.

      • Tap Add actions (B) to add new conditions.

  4. Tap Save to save the changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?