DUG_Infrascan Outdoor Motion Sensor 360_WH-00

LED indications

Pairing the device in Quick Home Connect

User Action

LED Indication

Status

Press the S/R button of the motion sensor 5 times in quick succession.

LED blinks green, once per second.

Pairing mode is active for 60 seconds. When pairing is completed, LED stops blinking.

Motion Detected

User Action

Status

LED Indication

When the motion is detected

The LED flashes red.

Resetting the Device

User Action

Status

LED Indication

Press the S/R (Setup/Reset) button 3 times within 0.5 seconds and then hold for 10 seconds

The red LED blinks for 10 seconds, flashes amber for 3 seconds, and then turns off.

→ (10 sec) → (3 sec)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?