Add to Post Queue

The Add to Post Queue tool is used in conjunction with Geodatabase Manager. It sends the current version to the post queue where Geodatabase Manager can post it as configured. The version must meet the following criteria before it can be posted:

  • NOT a Process Framework version (i.e., session or design)

  • NOT the SDE.Default version

To send a version to the Post Queue, follow the steps below. You may need to add the Add to Post Queue to a toolbar.

  1. Click the Add to Post Queue button.
  2. In the Submit to Post Queue window, select the version you'd like to send to the post queue.
  3. Set a priority value in the Priority field. A version with a higher priority (i.e., a higher number) is posted before versions with lower priority values (i.e., lower number). For example a version with a priority of 57 will post before a version with a priority of 4.
  4. Enter a post code in the Post Code field. This value must match the value set up in the Geodatabase Manager configuration, but it is not case sensitive (see the Configuration Guide topic Configure Post Process).
  5. Click Submit to add the version to the post queue.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.