Reconcile Session

An Approval Officer must reconcile a session in ArcMap before posting. This tool is not available in ArcFM Viewer for ArcGIS Engine. This function will reconcile the session's parent version to the current version. You must access Session Manager through ArcMap to reconcile a session. If necessary, a session may be reconciled any time after it has been created. If you are using an Access database, there isn't a parent version to be reconciled with. Therefore, the Reconcile button will not be enabled if you are working in a Access database.

  1. Open the session to be reconciled.
  2. On the Session Manager toolbar in ArcMap, click the Reconcile Session button.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.