Conductor Properties

Use Conductor properties to modify the conductor impedances used in the Voltage Drop and Fault Calculation.

To access the Conductor Properties menu, right-click a conductor in the Secondary Circuit Analysis window and select Properties from the resulting menu.

Here you can modify the conductor type and length to automatically recompute the impedance values. Uncheck the AutoCompute Impedances checkbox to modify resistance values for impedance.

NOTE: Secondary Circuit Analysis does not carry or recognize phase information on conductors. The number of phases on a conductor is determined by its transformer. This is true even if the conductor is imported from GIS and has GIS attributes indicating phase information or if conductor phasing information is present in the description field of the conductor lookup tables. Secondary Circuit Analysis ignores ALL phase information on a conductor and allows the transformer phases to imply the phases for the circuit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?