Similarities between Feeder Manager 1.0 and Feeder Manager 2.0

When using Feeder Manager 2.0, you should continue to use the following procedures and workflows used in Feeder Manager 1.0.

ArcFM Connect and Disconnect Tools:

When using Feeder Manager 2.0, continue to use the ArcFM Connect and Disconnect tool, and not Esri's Connect and Disconnect.

Adding Circuits:

The procedure for adding circuits in Feeder Manager 2.0 is the same as that for Feeder Manager 1.0. The procedure for adding subsources to your network is also the same for both versions of Feeder Manager.

Feeder Symbology:

The process of symbolizing on feeders is the same for both versions of Feeder Manager.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?