Conduit Manager Options

Conduit Manager Options are under the ArcMap Customize menu. Check these radio buttons to represent Conduit positions as either a rectangle or a circle. You can also choose a Cross Section component which displays the contents of a conduit visually in a layout view, as a contents list, or both.

  1. Select the Customize menu on the ArcMap toolbar.
  2. Select Conduit Manager Options.
  3. Select Rectangle or Circle.

  4. The Cross Section Components section allows you to modify which components are included when a cross section is placed.

    The Include Phase Designation in Cross Section checkbox, when checked, only affects cross section annotations that have yet to be placed. Existing cross section annotations are not changed by unchecking this option.

  5. Leader Line Settings allow you to edit the look of leader lines. Click OK.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?