Template Favorites

The Template Favorite tool is a powerful and flexible macro. With it you can create a construction sketch that precisely defines where to place sets of features concurrently on the map.

This section is divided in two: Design Template Favorite and Place Template Favorite.

Design Template Favorite : Focuses on the initial creation of a template. Many times, this task will be performed by an administrator.

Place Template Favorite : Focuses on template placement after it has been created.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?