Underground Facility Manager

The Underground Facility Manager (UFM) allows you to create and manage underground structures. Existing Conduit Manager tools allow you to create and configure a network of conduit and ducts within that conduit. UFM provides the ability to create and manage the underground structures that connect the conduit. You may create duct banks and ducts to which the conduit is associated. UFM provides the ability to assign conductors to duct banks and ducts.

Before using UFM, you may want to configure your Conduit System.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.