Create a model to export feeder information to CAD files

With slight modification, you can use the procedure above to export feeder data to .dxf or .dwg files, instead of .csv files. This option does not require third-party geoprocessing tools or scripts. You'll use the Export By Feeder tool in conjunction with Esri's Model Builder and an out-of-the-box Esri geoprocessing tool to accomplish this.

During step 5 in the previous procedure, substitute the Export to CAD tool for the Table To Excel script. this tool can be found in the ArcToolbox folder titled Conversion Tools > To CAD.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.