ArcFM Markup Pane

Publishes in Mobile config, Mobile Tools, Desktop using, EXI

Publishes in all
To display the markup pane, click the Markups button. Be aware that only active markups are displayed. Each markup record displays its current status, who submitted the markup, the date it was submitted, and a number of operational choices. From the markup pane, you can filter markups based on your assigned work, all available work, markup type, and markup name. You can also assign, unassign, or complete markup. For viewing specific markups on the map, there is functionality that allows you to zoom to a particular markup and show just that markup in the map.

Desktop Using and Mobile config and Mobile Tools
TIP: If your markup feature service is ArcGIS for Portal-federated, refer to Esri ’s Use ArcGIS Desktop with Your Portal topic to help you ensure that ArcMap is connected to the correct feature service.

Desktop Using and Mobile config and Mobile Tools

Desktop Using and Mobile config and Mobile Tools
IMPORTANT: If your markup map service operates over HTTPS, you may need to install the correct certificate on all Mobile client machines for markups to function properly.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.