Work Location Tabs
The user control for a Work Location offers two tabs for users to view information about a work location. The fields on these two tabs are not editable in Workflow Manager. You may open the design in ArcMap, select the work location on the Design tab, and edit its attributes.
Work Location
This tab provides information relating to the work location. Users may not edit this tab. To modify the Work Location Number or Description, open the design in ArcMap. Select the Work Location and edit the attribute values on the Attribute Editor Design tab. Click Update to save changes.
Field Descriptions
Work Location Number: This value uniquely identifies the work location within that design. This field may be edited in ArcMap.
Description: Allows the user to enter a description for the work location. This field may be edited in ArcMap.
Site Conditions
This tab allows you to enter and track Extended Data Management (EDM) information (see Using Designer for more information). You may open the design and edit this data on the Design tab. Site Conditions are not editable for a Work Location in Workflow Manager.
Field Descriptions
Labor Type: Indicates Internal or Contractor.
Network Status: Indicates the status of the network: Electric in Service, Gas in Service, or Not in Service.
Soil Condition: Indicates the soil condition: Firm, Hard, or Soft.
Traffic Condition: Indicates the amount of traffic in the area: High, Medium, Light, or No Traffic.